18.3.7.4 MPLAB XC32 Toolchain
The required macros for the MPLAB XC32 toolchain are:
- MP_PROCESSOR_OPTION - device name used by the compiler
- MP_LINKER_FILE_OPTION which can be one of two strings:
",—script=myScript32X.gld"– use this string if the project contains a linker script, in this case namedmyScript32X.gld.""– use the empty string if the project does not contain a linker script.
The optional macros for the MPLAB XC32 toolchain are:
- MP_EXTRA_CC_PRE
- MP_EXTRA_AS_PRE
- MP_EXTRA_AS_POST
- MP_EXTRA_AR_PRE (for lib project)
- MP_EXTRA_AR_POST (for lib project)
- MP_EXTRA_LD_PRE (for stand alone project)
- MP_EXTRA_LD_POST (for stand alone project)