14.24.2 Projects Window – Project Menu

Right click on a project name in the Projects window to pop up the Project menu. Menu items are shown in the tables below.

Table 14-92. Project Context Menu Items
Menu ItemDescription
BuildBuilds the project according to the options selected in the Project Properties window.
Note: When you Debug or Run, your project is built automatically.
Clean and BuildCleans and then builds the project according to the options selected in the Project Properties window.
Note: When you Debug or Run, your project is built automatically.
CleanCleans the project by deleting the outputs of previous builds.
Batch BuildBuilds one or more configurations.
Set ConfigurationDisplays project configurations for selection, or click Customize to open the Project Properties window to manage project configurations.
NewCreates a new item 
for MPLAB X IDE; embedded file types are available.

See New Submenu Items table below.

AddAdds an item 
for MPLAB X IDE; embedded file types are available.

See Add Submenu Items table below.

Set as Main ProjectSets this project as the main project.

This is useful when you are working with multiple projects.

FindFinds specific text in files in this project.
Locate HeadersLocates all the header files (.h) called out in the C code project files and presents them in a checklist window so they may be added to the project

There are several reasons why you might want to add headers to your project:

  • The files can be opened from the Projects window under Header Files instead of hunting for them on your computer.
  • The project created by Save Project As will not contain header files unless they are added to the project; therefore this project may not build if any user-generated header files are required.
  • The zipped project created by Package will not contain header files unless they are added to the project; therefore the unzipped project may not build if any user-generated header files are required.

This feature is able to locate user-generated header files for all Microchip toolchains.

RunExecutes the project code.
DebugExecutes the project code in a debug environment.
Step IntoSteps into Paused code running in the debug environment.
Make and Program DevicePrograms the target device and holds in Reset (do not run).
ProjectsSelect Project actions.

See Projects Submenu Items table below.

CloseCloses the selected project.
Open Required 
ProjectsLoads all other projects that are required for the selected project to run.
Code AssistanceSelects assistance in creating code: code folding, code completion, etc.
AnalysisDisplays list of analysis tools for selection.
Show Code Coverage SummaryOpens Code Coverage window to display summary.
VersioningControls the version of the project by using a version control system.
HistoryTo view, or revert to, the local history for the project.
PropertiesSets project properties.

For MPLAB X IDE, the Project Properties window is specific to embedded development.

Table 14-93. New Submenu Items
Menu ItemDescription
DirectoryOpens the New Directory dialog.

To view the new directory, see the Files window.

Note: To create a new logical folder, select Add > Add Logical Folder.
Compiler-specific header fileClick to create the compiler-specific header file template. For example, xc32_header.h.
Compiler-specific fileClick to create the compiler-specific file template. For example, xc32_newfile.c.
Text FileOpens the New Text File dialog.
OtherOpens the New File dialog.
Table 14-94. Add Submenu Items
Menu ItemDescription
Add Existing ItemAdds an existing file to the project.

The path to the file may be auto (selected by MPLAB X IDE), absolute or relative. Additionally, you may choose to copy the file into the project folder.

Add Existing Items from FoldersAdds all files contained in the specified folder(s).

You may also specify a pattern to ignore certain folders from inclusion. Click Default to see the default pattern. See also Tools > Options > Miscellaneous > Files, Files ignored by the IDE.

Add Logical FolderAdds a new logical folder to the Projects tree.
Note: To create an actual folder, select New > Directory.

To view the new directory, see the Files window.

Add External ItemAdds an existing item to the project.

The path to the file may be auto (selected by MPLAB X IDE), absolute or relative. Additionally, you may choose to copy the file into the project folder.

This is useful for adding simulator files, data sheet PDFs, and other files to the project for your reference.

Add autoload.pyAdds the autoload.py file to support scripting for devices supporting this feature.
Learn more about scriptingOpens the WebHelp topic Use IDE Scripting (autoload.py).
Table 14-95. Projects Submenu Items
Menu ItemDescription
PackagePackages the current project into a .zip file.
RenameRenames the project.
MoveMoves the project to another location.

Along with the project, it moves the source files that are inside the project directory. Files outside the project directory are not moved. However, the project still maintains reference to the files outside the project directory – this is by design.

CopyCreates a copy of the project.

If the source files are within the project directory, the source files are also copied to the new location. Files outside the project directory are not copied. However, the project still maintains reference to the files outside the project directory – this is by design.

DeleteDeletes the project files.

The project file is deleted but not the contents under the project directory. Only on selecting Also delete sources are all the source files deleted.

Export HexExports the project build as a Hex file.

In MPLAB IDE v8, export is an extraction of memory objects. In MPLAB X IDE, export is the hex file result of a build; therefore, it needs to include all necessary auxiliary memory settings for configuration and EEPROM in code.

If analyzing the exported hex file, use the device PIC file to decode extended linear address records.