14.24.4 Projects Window – Window Menu

Right click in an empty area in the Projects window to pop up the Window menu. The table below shows the specific menu items.

Table 14-97. Window Context Menu Items
Menu ItemDescription
New ProjectLaunches the New Project wizard.
New FileLaunches the New File wizard.
Open ProjectOpens an existing project.
Open Recent ProjectOpens an existing project for the list of recent projects.
Project GroupsOpens the Manage Groups dialog to select, create, remove or view project groups.
Build Project Name*Builds the selected project shown in parentheses.
Clean and Build Project Name*Cleans and Builds the selected project shown in parentheses.
Set Main ProjectSets the main project from the list of open projects.
Collapse AllCollapses all tree items.
Show Selected Node(s) Project OwnerSee NetBeans Help, Projects Window.
* Either name of project or “Main Project”