35.5.1.3.1 Self-Capacitance Sensor Arrangement

A self-capacitance sensor is connected to a single pin on the PTC through the Y-electrode. The PTC measures the capacitance of the sense electrode.

For a capacitive matrix array where only a single touch point is needed, self-capacitance sensing on both vertical and horizontal lines can effectively identify the touch point by locating the intersection of the touched lines.

Figure 35-5. Sensor Capacitance Sensor Arrangement

For more information about designing the touch sensor, refer to the AN2934—Capacitive Touch Sensor Design Guide (DS00002934).