3.3.12 PDS_UnRegFile
Definition: This function un-registers a file to the PDS. This makes the data stored in the NVM invalid and any operation on this file ID will be invalid after this point.
Syntax
PdsStatus_t PDS_UnRegFile(PdsFileItemIdx_t argFileId);
Input Parameters
|
Parameter Name |
Parameter Type |
Description |
|---|---|---|
argFileId | PdsFileItemIdx_t | PDS file ID of the item |
Return Type and Values
|
Parameter Name |
Parameter Type |
Description |
|---|---|---|
| ENUM | PDS status codes. Definition available in
|
|
Return Value |
Reason |
|---|---|
PDS_OK | PDS operation is success |
PDS_INVALID_FILE_IDX | File ID in the argument is not valid one |
API Type – Synchronous