2.2.7 RADIO_GetAttr
Definition: This function gets the stored value of the specified attribute.
Syntax
RadioError_t RADIO_GetAttr(RadioAttribute_t attribute, void *value);
Input Parameter
|
Parameter Name |
Parameter Type |
Description |
|---|---|---|
|
attribute |
RadioAttribute_t |
Structure for attribute list. Refer to Table 2-39 for a list of defined attribute names. |
Return Type and Values
|
Parameter Name |
Parameter Type |
Description |
|---|---|---|
| ENUM | Enumerated values containing all return types from radio layer |
|
Return Value |
Reason |
|---|---|
ERR_RADIO_BUSY | Radio is not in IDLE state |
ERR_NONE | Radio in IDLE state and stopping the continuous transmission |
API Type – Synchronous