5.2.1.4 I2C Interface
The I2C source streams the raw values received on the I2C interface.
The I2C Configuration options are displayed under the I2C interface in the DGI section of the left pane.
The I2C interface is under the DGI section of the Data Sources (left) pane. When an I2C connection is selected, the I2C settings are displayed in the lower section of this pane.
| Field Name | Values | Usage |
|---|---|---|
| Speed | 0 | The expected operation speed of the interface in Hertz helps the client device adjust the timings. Up to 400 kHz is supported. |
| Address | 1 | Address of the client device, 7-bit address : 8 to 120. |
| Kit-side Timestamping | Check to enable. | Target timestamping |