The Data Visualizer is included as part of the Atmel Studio installer, and can be
run either as a Studio extension or in Stand-Alone mode.
To run the Data Visualizer as an extension inside Atmel Studio, select it in
the Tools menu:
Kits supporting Data Visualizer functionality include a shortcut to the
extension on their start page in Atmel Studio.
If the stand-alone version of the Data Visualizer has been installed, look
for the shortcut in the Windows® start menu. The
stand-alone version is available for download from
gallery.microchip.com.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.