3.2.4 VOUT Target Supply
The Power Debugger can supply voltage to a target in the range of 1.6V to 5.5V, up to 100 mA. The voltage will be applied to the pin as shown in the silkscreen, and must be routed to the appropriate load by the user. VOUT can be set in a number of ways.
Important: VOUT setting is stored
in volatile memory on the Power Debugger. Toggling power
on the tool will result in VOUT being disconnected. This is done to protect the user’s
hardware.