23.11.2 TC2 Control Register B
| Name: | TCCR2B |
| Offset: | 0xB1 |
| Reset: | 0x00 |
| Property: | - |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| FOC2A | FOC2B | WGM2 [2] | CS2[2:0] | ||||||
| Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | |||
Bit 7 – FOC2A Force Output Compare A
The FOC2A bit is only active when the WGM bits specify a non-PWM mode.
To ensure compatibility with future devices, this bit must be set to zero when TCCR2B is written when operating in PWM mode. When writing a logical one to the FOC2A bit, an immediate Compare Match is forced on the Waveform Generation unit. The OC2A output is changed according to its COM2A[1:0] bits setting. Note that the FOC2A bit is implemented as a strobe. Therefore it is the value present in the COM2A[1:0] bits that determines the effect of the forced compare.
A FOC2A strobe will not generate any interrupt, nor will it clear the timer in CTC mode using OCR2A as TOP.
The FOC2A bit is always read as zero.
Bit 6 – FOC2B Force Output Compare B
The FOC2B bit is only active when the WGM bits specify a non-PWM mode.
To ensure compatibility with future devices, this bit must be set to zero when TCCR2B is written when operating in PWM mode. When writing a logical one to the FOC2B bit, an immediate Compare Match is forced on the Waveform Generation unit. The OC2B output is changed according to its COM2B[1:0] bits setting. Note that the FOC2B bit is implemented as a strobe. Therefore it is the value present in the COM2B[1:0] bits that determines the effect of the forced compare.
A FOC2B strobe will not generate any interrupt, nor will it clear the timer in CTC mode using OCR2B as TOP.
The FOC2B bit is always read as zero.
Bit 3 – WGM2 [2] Waveform Generation Mode
Bits 2:0 – CS2[2:0] Clock Select 2 [n = 0..2]
The three Clock Select bits select the clock source to be used by the Timer/Counter.
| CA22 | CA21 | CS20 | Description |
|---|---|---|---|
| 0 | 0 | 0 | No clock source (Timer/Counter stopped). |
| 0 | 1 | clkI/O/1 (No prescaling) | |
| 0 | 1 | 0 | clkI/O/8 (From prescaler) |
| 0 | 1 | 1 | clkI/O/32 (From prescaler) |
| 1 | 0 | 0 | clkI/O/64 (From prescaler) |
| 1 | 0 | 1 | clkI/O/128 (From prescaler) |
| 1 | 1 | 0 | clkI/O/256 (From prescaler) |
| 1 | 1 | 1 | clkI/O/1024 (From prescaler) |
If external pin modes are used for the Timer/Counter0, transitions on the T0 pin will clock the counter even if the pin is configured as an output. This feature allows software control of the counting.