3.5.2 Import AVR® Studio 4 Project
Click the menu File → Import → AVR® Studio 4 Project.. or Ctrl+4.

An Import AVR Studio 4 Project dialog will appear.
Type the name of your project or browse to the project location by clicking the Browse button of the APS file location tab.

Microchip Studio will proceed with the conversion, giving updates on the progress. Warnings and errors will show in the Summary window.
Check the Show conversion log after this page is closed to view the complete conversion log.
Click Finish to access your newly converted project.


Note: Currently - the conversion
only adds a project file and solution file if the Solution Folder is the same as the APS
File Location. No other files will be modified.