3.1.8.1 Change Version
Components are versioned when added to the project. To change the version used, use this dialog.
There are two options when choosing the component version:
- Use a specific version
- Lock the project to a specific version of the component.
- Use the latest version
- Choose the most recent version of the available component.

Components are part of the device packs in Microchip Studio. Manage these device packs using the Device Pack Manager.