3.2.4 Starting a New GCC Project for SAM Device

  1. Create a new project by selecting New Project from the Project menu. This will open the Project Wizard.
  2. Select C/C++ → GCC C Executable Project as a template. Then, specify a project name, select a location, and write a solution name for the project. Some start-up files will be added to the project by default, which will contain some device-specific functions and libraries. Press OK when you are satisfied with the settings.
  3. Select C/C++ → GCC C Static Library Project as a template. Then, specify a project name, select a location, and write a solution name for the project. This creates a Static Library (LIB) project, which is a great way to reuse code.
    Tip:

    See section Static Library Project to learn more about Static Library projects.

  4. A device selection table will appear. Choose the device family as SAM3 or SAM4 and select the target platform for your project. To start, you can choose the ATSAM3S1A device.
  5. The project tree will be set up. Notice the addition of the initial files created in step 2 to the project node. Also, the file containing the main() function opens in the editor.

    Here is a list of files that will be created:

    • A file with the same name as the project will, by default, be created and added to the project. It will contain the main() function.
    • A startup file(startup_*.c) will be available at 'cmsis\src' directory. It contains the default interrupt handlers for all the peripherals.
    • A system file(system_*.c) available at 'cmsis\src' provides the system-level initialization functions that are called on start-up
    • Linker scripts with appropriate sections based on the device will be created at the 'cmsis\LinkerScripts' directory in the project folder
    • If you have deleted any files in the cmsis folder and want to revert it or changed the device, just right click the Project and click 'CMSIS Update from Microchip' to get the appropriate files.
    Note: It is recommended not to change the contents of the startup_*.c and system_*.c files unless you have no other choice. These start-up, system, and linker scripts will not be created for Arm static library projects.
  6. You can also use the Driver Selection Wizard, invoked from Project → ASF Wizard, to facilitate applications development and verification.
    In the ASF Wizard, you can select which Drivers, Components, and Services you would like to use in the project for the current build architecture and board.
  7. Now, write the following code into the open editor window:
    #define MAXINT 200000
    
    int main(void) 
    {
        unsigned int t=1000, k=0, l=5, pn=2; 
        unsigned int primes[t];
        primes[0]=2;
        primes[1]=3;
    
        while (pn < t || primes[pn] < MAXINT)
        {
            for ( k = 0; k <= pn; k++)
            {
                if (l % primes[k] == 0)
    			{
                    goto otog;
    			}
                else 
                {
                    if (k == pn)
                        primes[pn++]=l;
                } 
            }
    otog:
            l += 2;
        }
        return 0;
    }
  8. Build the project.