10.4.1 Managing Code Snippets
To Access the Code Snippets Manager
On the Tools menu, click Code Snippets Manager.
To Add a Directory To the Code Snippet Manager
- In the Language: Drop-down list, select the language you want to add a directory to.
- Click Add. This opens the Code Snippets Directory window.
- Select the directory you want to add to the Code Snippets Manager and click OK. The directory will now be used to search for available code snippets.
To Remove a Directory From the Code Snippet Manager
- Select the directory that you want to remove.
- Click Remove.
To Import a Code Snippet Into the Code Snippet Manager
- In the Language: drop-down list, select the language you want to add the code snippet to.
- Select the existing folder you want to place the imported code snippet into.
- Click Import. This opens the Code Snippets Directory window.
- Select the code snippet file you want to add to the Code Snippets Manager and click OK. The code snippet is now available for insertion into the code editor.