9.6.2 Overview of the QTouch® Project Builder

Getting Started With the QTouch® Composer in Microchip Studio on YouTube.
QTouch Project builder will guide you through all steps from selecting device and touch sensors to automatically generating a complete touch project.
- Start Microchip Studio.
- Open the File menu. Click on 'New → Project'.

- The 'New Project' dialog is opened. Select 'GCC C
QTouch Executable Project' in the New Project dialog.

Enter the following details in the 'New Project' dialog and click the OK button:
- Name of the project
- Location of the project and solution
- Name of the solution
- The 'QTouch Project Builder' wizard is opened, which will guide you through the steps involved in creating a project.