1.2.9.1 SYS_PORT_PinWrite Function
C
void SYS_PORT_PinWrite(SYS_PORT_PIN pin, bool value)Summary
Writes to the selected pin.
Description
This function writes/drives the "value" on the selected I/O line/pin.
Precondition
Port Initialization must have been done using appropriate Initialize API call.
Parameters
| Param | Description |
|---|---|
| pin | One of the IO pins from the enum SYS_PORT_PIN |
| value | value to be written on the selected pin: |
- true: set pin to high (1).
- false: clear pin to low (0).
Returns
None.
Example
SYS_PORT_PinWrite(SYS_PORT_PIN_PB3, true);
Remarks
None.