1.2.9.3 SYS_PORT_PinLatchRead Function
C
bool SYS_PORT_PinLatchRead ( SYS_PORT_PIN pin )
Summary
Read the value driven on the selected pin.
Description
This function reads the data driven on the selected I/O line/pin. Whatever data is written/driven on I/O line by using any of the PORTS APIs, will be read by this API.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| pin | One of the IO pins from the enum SYS_PORT_PIN |
Returns
Returns the value driven on the selected I/O pin.
Example
bool value; value = SYS_PORT_PinLatchRead(SYS_PORT_PIN_PB3);
Remarks
To read actual pin value, SYS_PORT_PinRead API should be used.