1.1.11.1 AT25 Driver
This driver provides a non-blocking interface to read and write to the external AT25 EEPROM. The library uses the SPI peripheral library (PLIB) to interface with the AT25
Key Features:
Supports a single instance of the AT25 EEPROM and a single client to the driver
Supports page writes
Supports writes to random memory address within page boundaries
The library interface is compliant to the block media interface expected by the Memory Driver. This allows running a file system on the AT25 EEPROM using the Memory Driver and the File System Service
The library can be used in both Bare-Metal and RTOS environments