1.4.4.11 OSAL_MUTEX_Lock Function
C
OSAL_RESULT OSAL_MUTEX_Lock(OSAL_MUTEX_HANDLE_TYPE* mutexID, uint16_t waitMS)Summary
Locks a mutex.
Description
This function locks a mutex, waiting for the specified time-out. If it cannot be obtained or the time-out period elapses 'false' is returned.
Precondition
Mutex must have been created.
Parameters
| Param | Description |
|---|---|
| mutexID | Pointer to the mutex handle |
| waitMS | Time-out value in milliseconds: 0 - do not wait return immediately, OSAL_WAIT_FOREVER - wait until mutex is obtained before returning, Other values - time-out delay |
Returns
OSAL_RESULT_TRUE - Mutex successfully obtained
OSAL_RESULT_FALSE - Mutex failed to be obtained or time-out occurred
Example
...
if (OSAL_MUTEX_Lock(&mutexData, 1000) == OSAL_RESULT_TRUE)
{
// manipulate the shared data
...
// unlock the mutex
OSAL_MUTEX_Unlock(&mutexData);
}Remarks
None.