1.2.8.4 SYS_INT_Restore Function
C
void SYS_INT_Restore( bool state )Summary
Restores the interrupt controller to the state specified in the parameter.
Description
This function restores the interrupt controller to the state specified in the parameters.
Precondition
SYS_INT_Disable must have been called to get previous state of the global interrupt.
Parameters
| Param | Description |
|---|---|
| - true | Enable Global Interrupt |
| - false | Disable Global Interrupt |
Returns
None.
Example
bool interruptState;
// Save global interrupt state and disable interrupt
interruptState = SYS_INT_Disable();
// Critical Section
// Restore interrupt state
SYS_INT_Restore(interruptState)Remarks
None.