1.1.10.1.2 Using The Library
The AT24 driver provides non-blocking API's to read, write AT24 EEPROM.
The AT24 driver can be used in following ways:
To perform reads and writes from/to any EEPROM memory address, with number of bytes spanning multiple pages
To perform page write to AT24 EEPROM. Here, the memory start address must be aligned to the page boundary
To interface with the Memory driver to perform block operations on the AT24 EEPROM
Application can either register a callback to get notified once the data transfer is complete or can poll the status of the data transfer
Example application to Write and Read AT24 EEPROM
#define BUFFER_SIZE 512 #define MEM_ADDRESS 0x0 APP_DATA CACHE_ALIGN appData; static uint32_t erase_index = 0; static uint32_t write_index = 0; static void APP_EEPROM_EventHandler(DRV_AT24_TRANSFER_STATUS event, uintptr_t context) { switch(event) { case DRV_AT24_TRANSFER_STATUS_COMPLETED: { appData.isTransferDone = true; break; } case DRV_AT24_TRANSFER_STATUS_ERROR: default: { appData.isTransferDone = false; appData.state = APP_STATE_ERROR; break; } } } void APP_Initialize ( void ) { uint32_t i = 0; /* Place the App state machine in its initial state. */ appData.state = APP_STATE_INIT; for (i = 0; i < BUFFER_SIZE; i++) { appData.writeBuffer[i] = i; } appData.isTransferDone = false; } void APP_Tasks ( void ) { uint32_t i; /* Check the application's current state. */ switch ( appData.state ) { /* Application's initial state. */ case APP_STATE_INIT: { appData.drvHandle = DRV_AT24_Open(DRV_AT24_INDEX, DRV_IO_INTENT_READWRITE); if (appData.drvHandle != DRV_HANDLE_INVALID) { DRV_AT24_EventHandlerSet(appData.drvHandle, APP_EEPROM_EventHandler, 0); appData.state = APP_STATE_WRITE; } else { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_WRITE: { /* Set the next state first as callback may be fired before the state * is changed; potentially over-writing error state set from the callback */ appData.state = APP_STATE_WAIT_WRITE_COMPLETE; if (DRV_AT24_Write(appData.drvHandle, appData.writeBuffer, BUFFER_SIZE, AT24_EEPROM_MEM_ADDR) == false) { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_WAIT_WRITE_COMPLETE: { if (appData.isTransferDone == true) { appData.isTransferDone = false; appData.state = APP_STATE_READ; } break; } case APP_STATE_READ: { appData.state = APP_STATE_WAIT_READ_COMPLETE; if (DRV_AT24_Read(appData.drvHandle, appData.readBuffer, BUFFER_SIZE, AT24_EEPROM_MEM_ADDR) == false) { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_WAIT_READ_COMPLETE: { if (appData.isTransferDone == true) { appData.isTransferDone = false; appData.state = APP_STATE_VERIFY; } break; } case APP_STATE_VERIFY: { if (memcmp(appData.writeBuffer, appData.readBuffer, BUFFER_SIZE ) == 0) { appData.state = APP_STATE_SUCCESS; } else { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_SUCCESS: { appData.state = APP_STATE_IDLE; break; } case APP_STATE_ERROR: { appData.state = APP_STATE_IDLE; break; } case APP_STATE_IDLE: DRV_AT24_Close(appData.drvHandle); default: { break; } } }