1.1.11.1 AT24 Driver
This driver provides a non-blocking interface to read and write to external AT24 EEPROM. The library uses the I2C Peripheral Library (PLIB) to interface with the AT24.
Key features:
-
Supports a single instance of the AT24 EEPROM and a single client to the driver.
-
Supports page writes.
-
Supports writes to random memory address within page boundaries.
-
The library interface is compliant to the block media interface expected by the Memory driver. This allows running a file system on the AT24 EEPROM using the Memory Driver and the File System Service.
-
The library can be used in both Bare-Metal and RTOS environments.