1.1.11.1.2 Using the Library
The AT24 driver provides non-blocking APIs to read, write AT24 EEPROM.
The AT24 driver can be used in following ways:
-
To perform reads and writes from/to any EEPROM memory address, with number of bytes spanning multiple pages
-
To perform page write to AT24 EEPROM. Here, the memory start address must be aligned to the page boundary
-
To interface with the Memory driver to perform block operations on the AT24 EEPROM
-
Application can either register a callback to get notified once the data transfer is complete or can poll the status of the data transfer
Example Application to Write and Read AT24 EEPROM
#define BUFFER_SIZE 512 #define MEM_ADDRESS 0x0 APP_DATA CACHE_ALIGN appData; static uint32_t erase_index = 0; static uint32_t write_index = 0; static void APP_EEPROM_EventHandler(DRV_AT24_TRANSFER_STATUS event, uintptr_t context) { switch(event) { case DRV_AT24_TRANSFER_STATUS_COMPLETED: { appData.isTransferDone = true; break; } case DRV_AT24_TRANSFER_STATUS_ERROR: default: { appData.isTransferDone = false; appData.state = APP_STATE_ERROR; break; } } } void APP_Initialize ( void ) { uint32_t i = 0; /* Place the App state machine in its initial state. */ appData.state = APP_STATE_INIT; for (i = 0; i < BUFFER_SIZE; i++) { appData.writeBuffer[i] = i; } appData.isTransferDone = false; } void APP_Tasks ( void ) { uint32_t i; /* Check the application's current state. */ switch ( appData.state ) { /* Application's initial state. */ case APP_STATE_INIT: { appData.drvHandle = DRV_AT24_Open(DRV_AT24_INDEX, DRV_IO_INTENT_READWRITE); if (appData.drvHandle != DRV_HANDLE_INVALID) { DRV_AT24_EventHandlerSet(appData.drvHandle, APP_EEPROM_EventHandler, 0); appData.state = APP_STATE_WRITE; } else { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_WRITE: { /* Set the next state first as callback may be fired before the state * is changed; potentially over-writing error state set from the callback */ appData.state = APP_STATE_WAIT_WRITE_COMPLETE; if (DRV_AT24_Write(appData.drvHandle, appData.writeBuffer, BUFFER_SIZE, AT24_EEPROM_MEM_ADDR) == false) { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_WAIT_WRITE_COMPLETE: { if (appData.isTransferDone == true) { appData.isTransferDone = false; appData.state = APP_STATE_READ; } break; } case APP_STATE_READ: { appData.state = APP_STATE_WAIT_READ_COMPLETE; if (DRV_AT24_Read(appData.drvHandle, appData.readBuffer, BUFFER_SIZE, AT24_EEPROM_MEM_ADDR) == false) { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_WAIT_READ_COMPLETE: { if (appData.isTransferDone == true) { appData.isTransferDone = false; appData.state = APP_STATE_VERIFY; } break; } case APP_STATE_VERIFY: { if (memcmp(appData.writeBuffer, appData.readBuffer, BUFFER_SIZE ) == 0) { appData.state = APP_STATE_SUCCESS; } else { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_SUCCESS: { appData.state = APP_STATE_IDLE; break; } case APP_STATE_ERROR: { appData.state = APP_STATE_IDLE; break; } case APP_STATE_IDLE: DRV_AT24_Close(appData.drvHandle); default: { break; } } }