DRV_AT25_Read Function

C

bool DRV_AT25_Read(const DRV_HANDLE handle, void *rxData, uint32_t rxDataLength, uint32_t address )

Summary

Reads 'n' bytes of data from the specified start address of EEPROM.

Description

This function schedules a non-blocking read operation for the requested number of data bytes from the given address of the EEPROM.

The requesting client should call DRV_AT25_TransferStatusGet API to know the current status of the request OR the requesting client can register a callback function with the driver to get notified of the status.

Precondition

DRV_AT25_Open must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine
rxDataBuffer pointer into which the data read from the DRV_AT25 Flash memory will be placed
rxDataLengthTotal number of bytes to be read
addressMemory start address from where the data should be read

Returns

True:
  • if the read request is accepted
False:
  • if handle is invalid
  • if the pointer to the receive buffer is NULL or number of bytes to read is 0
  • if the driver is busy handling another transfer request

Example

#define BUFFER_SIZE 1024
#define MEM_ADDRESS 0x00

uint8_t readBuffer[BUFFER_SIZE];

// myHandle is the handle returned from DRV_AT25_Open API.
// In the below example, the transfer status is polled. However, application can
// register a callback and get notified when the transfer is complete.

if (DRV_AT25_Read(myHandle, readBuffer, BUFFER_SIZE, MEM_ADDRESS) != true)
{
    // Error handling here
}
else
{
    // Wait for read to be completed
    while(DRV_AT25_TransferStatusGet(myHandle) == DRV_AT25_TRANSFER_STATUS_BUSY);
}

Remarks

None.