DRV_AT25_Status Function

C

SYS_STATUS DRV_AT25_Status( const SYS_MODULE_INDEX drvIndex )

Summary

Gets the current status of the AT25 driver module.

Description

This routine provides the current status of the AT25 driver module.

Preconditions

Function DRV_AT25_Initialize should have been called before calling this function.

Parameters

ParametersDescription
drvIndexIdentifier for the instance used to initialize driver

Returns

SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.

SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.

Example

SYS_STATUS status;

status = DRV_AT25_Status(DRV_AT25_INDEX);

if (status == SYS_STATUS_READY)
{
    // AT25 driver is initialized and ready to accept requests.
}

Remarks

None.