1.1.2.4.5 DRV_I2C_TransferSetup Function
C
bool DRV_I2C_TransferSetup ( DRV_HANDLE handle, DRV_I2C_TRANSFER_SETUP* setup )
Summary
Sets the dynamic transfer setup of the driver.
Description
This function should be used to update any of the DRV_I2C_TRANSFER_SETUP parameters for the selected client of the driver dynamically. It is mainly helpful for multi-client scenario where different clients need different setup, such as clock speed. The DRV_I2C_TransferSetup function must be called before submitting any I2C driver read/write requests.
Precondition
DRV_I2C_Open must have been called to obtain a valid opened device handle.
In case of asynchronous driver, all transfer requests from the queue must have been processed.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| setup | Pointer to the structure containing the new configuration settings |
Returns
None.
Example
// myI2CHandle is the handle returned by the DRV_I2C_Open function.
DRV_I2C_TRANSFER_SETUP setup;
setup.clockSpeed = 400000;
DRV_I2C_TransferSetup ( myI2CHandle, &setup );Remarks
None.