1.1.4.2 Using the Library
The NAND Flash driver provides the blocking APIs to read, write and erase NAND Flash memory.
The NAND Flash driver can be used in following ways:
-
To perform page and block write to NAND Flash
-
To perform page and block read from NAND Flash
-
To perform block erase operation
-
To read Flash identifier codes, Parameter page and geometry of the NAND Flash
-
To reset the Flash device and enable/disable target specific features
-
To check whether NAND Flash block is bad or good, and tag the NAND Flash block to bad or good
Example Application to Erase, Write and Read NAND Flash Memory
#define PAGE_SIZE 4096 #define SPARE_SIZE 224 #define BUFFER_SIZE (PAGE_SIZE + SPARE_SIZE) #define NAND_FLASH_ADDR_ONFI_SIGNATURE 0x20 static APP_DATA appData; static uint16_t blockNum = 3; static uint16_t pageNum = 0; static char *ptrReadId = 0; void APP_Initialize ( void ) { uint32_t i = 0; /* Place the App state machine in its initial state. */ appData.state = APP_STATE_INIT; for (i = 0; i < PAGE_SIZE; i++) { appData.writeBuffer[i] = i; } } void APP_Tasks ( void ) { /* Check the application's current state. */ switch ( appData.state ) { /* Application's initial state. */ case APP_STATE_INIT: { if (DRV_NAND_FLASH_Status(DRV_NAND_FLASH_INDEX) == SYS_STATUS_READY) { appData.state = APP_STATE_OPEN_DRIVER; } break; } case APP_STATE_OPEN_DRIVER: { appData.handle = DRV_NAND_FLASH_Open((SYS_MODULE_INDEX)DRV_NAND_FLASH_INDEX, DRV_IO_INTENT_READWRITE); if (appData.handle != DRV_HANDLE_INVALID) { appData.state = APP_STATE_ID_GET; } break; } case APP_STATE_ID_GET: { if (DRV_NAND_FLASH_IdRead(appData.handle, &appData.readId, NAND_FLASH_ADDR_ONFI_SIGNATURE) != true) { appData.state = APP_STATE_ERROR; } else { ptrReadId = (char *)&appData.readId; if (ptrReadId[0] == 'O' && ptrReadId[1] == 'N' && ptrReadId[2] == 'F' && ptrReadId[3] == 'I') { appData.state = APP_STATE_GEOMETRY_GET; } } break; } case APP_STATE_GEOMETRY_GET: { if (DRV_NAND_FLASH_GeometryGet(appData.handle, &appData.geometry) != true) { appData.state = APP_STATE_ERROR; } else { appData.state = APP_STATE_ERASE_FLASH; } break; } case APP_STATE_ERASE_FLASH: { if (DRV_NAND_FLASH_SkipBlock_BlockErase(appData.handle, blockNum, 0) != true) { appData.state = APP_STATE_ERROR; } else { appData.state = APP_STATE_WRITE_MEMORY; } break; } case APP_STATE_WRITE_MEMORY: { if (DRV_NAND_FLASH_SkipBlock_PageWrite(appData.handle, blockNum, pageNum, appData.writeBuffer, 0, false) != true) { appData.state = APP_STATE_ERROR; } else { appData.state = APP_STATE_READ_MEMORY; } break; } case APP_STATE_READ_MEMORY: { if (DRV_NAND_FLASH_SkipBlock_PageRead(appData.handle, blockNum, pageNum, appData.readBuffer, 0, false) != true) { appData.state = APP_STATE_ERROR; } else { appData.state = APP_STATE_VERIFY_DATA; } break; } case APP_STATE_VERIFY_DATA: { if (!memcmp(appData.writeBuffer, appData.readBuffer, appData.geometry.pageSize)) { appData.state = APP_STATE_SUCCESS; } else { appData.state = APP_STATE_ERROR; } break; } case APP_STATE_SUCCESS: { DRV_NAND_FLASH_Close(appData.handle); appData.state = APP_STATE_IDLE; break; } case APP_STATE_ERROR: case APP_STATE_IDLE: default: break; } }