5.4.2.2 Routing and Socket Card
Place the routing card above the motherboard and make sure that the white spot in the corner matches the white spot on the motherboard. The small plastic taps on the ends of the spring-loaded connectors should mate with the holes in the routing card. When the routing card is in the correct position, place the socket card onto the routing card with the white spot matching the one on the routing card. Make sure that the plastic taps on the connectors on the socket card mates with the routing card as well.
Insert the four screws and tighten them firmly into the nuts.