1.4.3.4 PAL_PLC_Deinitialize Function
C
void PAL_PLC_Deinitialize(SYS_MODULE_OBJ object);Summary
De-initializes the specified instance of the PLC PAL module.
Description
This function de-initializes the specified instance of the PLC PAL module, disabling its operation and invalidates all of the internal data.
Precondition
Function PAL_PLC_Initialize must have been called before calling this routine and a valid SYS_MODULE_OBJ must have been returned.
Parameters
| Param | Description |
|---|---|
| object | PLC PAL module object handle, returned by PAL_PLC_Initialize. |
Returns
None.
Example
// This code example shows how the PLC PAL can be deinitialized. // It is assumed the PLC PAL module was already initialized. SYS_MODULE_OBJ palPlcobj; PAL_PLC_Deinitialize(palPlcobj);
Remarks
Once PAL_PLC_Initialize has been called, PAL_PLC_Deinitialize must be called before PAL_PLC_Initialize can be called again.