1.4.3.17 PAL_PLC_RxParamsIndication Typedef
C
typedef void (*PAL_PLC_RxParamsIndication)(MAC_RT_RX_PARAMETERS_OBJ *pParameters);
Summary
Pointer to a PLC PAL event handler function to get parameters from the last received message.
Description
This data type defines the required function signature for the PLC PAL reception parameters event handling callback function. When PAL_PLC_Initialize is called, a client must register a pointer whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive transfer related event calls back from the PLC PAL.
The parameters and return values are described here and a partial example implementation is provided.
Parameters
| Param | Description |
|---|---|
| pParameters | Pointer to the parameters of the last received message. |
Returns
None.
Example
static MAC_RT_RX_PARAMETERS_OBJ rxParameters;
static void _plcRxParamsIndication(MAC_RT_RX_PARAMETERS_OBJ *pParameters)
{
// extract all parameters from received message
memcpy(rxParameters, pParameters, sizeof(MAC_RT_RX_PARAMETERS_OBJ));
}
PAL_PLC_INIT palPlcInitData;
SYS_MODULE_OBJ palPlcObj;
palPlcInitData.macRtBand = G3_FCC;
palPlcInitData.macRtHandlers.palPlcDataIndication = _plcDataIndication;
palPlcInitData.macRtHandlers.palPlcTxConfirm = _plcTxConfirm;
palPlcInitData.macRtHandlers.palPlcCommStatusIndication = _plcCommStatusIndication;
palPlcInitData.macRtHandlers.palPlcRxParamsIndication = _plcRxParamsIndication;
palPlcInitData.initMIB = true;
// Initialize the PLC PAL module
palPlcObj = PAL_PLC_Initialize(PAL_PLC_PHY_INDEX, (const SYS_MODULE_INIT *) &palPlcInitData);Remarks
This handler function is called before the data indication callback.