1.5.3.2 PAL_RF_Status Function
C
PAL_RF_STATUS PAL_RF_Status(SYS_MODULE_OBJ object);Summary
Returns status of the specific instance of the RF PAL module.
Description
This function returns the status of the specific RF PAL module instance.
Precondition
The PAL_RF_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | RF PAL object handle, returned from PAL_RF_Initialize. |
Returns
- PAL_RF_STATUS_READY: Indicates that the module is initialized and is ready to accept new requests from the client.
- PAL_RF_STATUS_BUSY: Indicates that the module is busy with a previous initialization request from the client.
- PAL_RF_STATUS_ERROR: Indicates that the module is in an error state. Any value lower than SYS_STATUS_ERROR is also an error state.
- PAL_RF_STATUS_UNINITIALIZED: Indicates that the module is not initialized.
Example
// "object" returned from PAL_RF_Initialize
PAL_RF_STATUS palRfStatus;
palRfStatus = PAL_RF_Status (object);
if (palRfStatus == PAL_RF_STATUS_READY)
{
// RF PAL is initialized and is ready to accept client requests.
}Remarks
The upper layer must ensure that PAL_RF_Status returns PAL_RF_STATUS_READY before performing PAL RF operations.