2.6 VCC
When programming the target microcontroller, the programmer outputs need to stay within the ranges specified in the DC Characteristics.
To easily adapt to any target voltage, the programmer can draw all power required from the target system. This is allowed as the In-System Programmer will draw very little power from the target system, typically no more than 20mA. The programmer shown in this application note operates in this mode.
As an alternative, the target system can have its power supplied from the programmer through the same connector used for the communication. This would allow the target to be programmed without applying power to the target externally.
| Pin | Recommendation |
|---|---|
| GND | Connect ground of the target to ground of the In-System Programmer |
| RESET | Allow the In-System Programmer to Reset the target system |
| SCK | When the target AVR microcontroller reset is active, this
line should be controlled by the ISP Programmer. Note: Edges on this line
after Reset is pulled low, will be critical and cause the target AVR
microcontroller to lose synchronization with the
programmer. When programming, oscillations on this pin should be
tolerated by the surrounding system when the AVR Reset is
active. |
| MOSI | When the target AVR microcontroller Reset is active, this line should be controlled by the ISP Programmer. When programming, oscillations on this pin should be tolerated by the surrounding system when the AVR Reset is active. |
| MISO | When the target AVR microcontroller Reset is active, this line should be allowed to become an output. When programming, oscillations on this pin should be tolerated by the surrounding system when the AVR Reset is active. |
| VCC | Allow the In-System Programmer to draw power from the target system, to adapt to any allowed target voltage. The maximum current needed to power the programmer will vary depending on the programmer being used. |