8.2.4 Storage Area Flash (SAF) Lock Enable
The SAFLOCK Configuration bit allows for one-time programmability of the
Storage Area Flash (SAF). This bit can only be enabled once. Once enabled, this bit
cannot be disabled (even through a Bulk Erase operation) and locks the designated SAF
area and the SAFSZ bits. When SAFSZ is
enabled, the SAF locked area can only be increased in size by programming a
SAFSZ bit to ‘0’. However, once programmed
to ‘0’, either through ICSP or a self-write, the SAF locked area cannot
be reduced in size since the bits can never be erased to a ‘1’, not
even through a Bulk Erase. When SAFLOCK is enabled, the SAF
area becomes write protected and an NVM write error is set during self-writes. Setting
the SAFLOCK Configuration bit requires a specific unlock
sequence that is described below, but is also covered in more detail in the Family
Programming Specification document for the specific device.
- Setting the
SAFLOCK Configuration bit through the ICSP
interface requires the following sequence:
- Send Program Access Enable Command with appropriate payload. For more information on the Program Access Enable Command, refer to the PIC18-Q24 Family Programming Specification.
- Send Program Data Command to write to the SAFLOCK bit. For more information on the Program Data Command, refer to the PIC18-Q24 Family Programming Specification.