9.3 NAND Flash Memory
The Microchip SAM9X75 System-On-Module Series embeds an SLC NAND Flash memory supported through its External Bus Interface controller with different memory sizes depending on the part number.
- Either one of the above references can be mounted on the Microchip SAM9X75 System-On-Module Series.
- Read/write speed may vary depending on the NAND Flash reference fitted to the module.
For more information about NAND Flash memories, refer to the relevant data sheets (see Reference Documents).
Microchip Linux distribution supports all references. For details on how to build Linux software, refer to www.linux4microchip.com.
NAND_CS_IN (pin 17) is accessible externally and can be uncoupled from NAND_CS_PD4 (pin 18) so that the boot can be unselected from the NAND Flash memory during debug phases.