43.3.7.3 Point Doubling
Purpose
This service is used to perform a Point Doubling, based on a given elliptic curve over GF(2n).
How to Use the Service
Description
The operation performed is:
PtC = 2 × PtA
In this computation, the following parameters need to be provided:
- A the input point is filled in projective coordinates (X,Y,Z) (pointed by {nu1PointABase,3*u2ModLength + 12}). This point can be the Infinite Point.
- Cns the Fast Modular Constant filled (pointed by {nu1CnsBase,u2ModLength +8})
- P the modulus filled (pointed by {nu1ModBase,u2ModLength +4})
- The workspace not initialized (pointed by {nu1WorkSpace, 4*u2ModLength +28}
- The a and b Parameters relative to the Elliptic Curve Equation (pointed by {nu1ABBase,2*u2ModLength+ 8})
- The resulting C point is represented in projective coordinates (X,Y,Z) and is stored at the very same place than the input point A. This point can be the Infinite Point.
The service name for this operation is
GF2NEccDblFast
. This service uses Fast mode
and Fast Modular Reduction for computation.
Important: Before using
this service, ensure that the constant Cns has been calculated
with the setup of the Fast Modular Reductions service.
Parameters Definition
Parameter | Type | Direction | Location | Data Length | Before Executing the Service | After Executing the Service |
---|---|---|---|---|---|---|
nu1ModBase | nu1 | I | Crypto RAM | u2ModLength + 4 | Base of modulus P | Base of modulus P |
nu1CnsBase | nu1 | I | Crypto RAM | u2ModLength + 12 | Base of Cns | Base of Cns |
u2ModLength | u2 | I | – | – | Length of modulus P | Length of modulus P |
nu1ABBase | u2 | I | Crypto RAM | 2*u2ModLength + 8 | Parameters a and b of the elliptic curve | Parameter a and b of the elliptic curve |
nu1PointABase | nu1 | I/O | Crypto RAM | 3*u2ModLength + 12 | Input point A (projective coordinates) | Resulting point C (projective coordinates) |
nu1Workspace | nu1 | I | Crypto RAM | 4*u2ModLength + 28 | – | Corrupted workspace |
Code Example
PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;
PUKCL (u2Option) = 0;
PUKCL _GF2NEccDbl(nu1ModBase) = <Base of the ram location of P>;
PUKCL _GF2NEccDbl(u2ModLength) = <Byte length of P>;
PUKCL _GF2NEccDbl(nu1CnsBase) = <Base of the ram location of Cns>;
PUKCL _GF2NEccDbl(nu1PointABase) = <Base of the ram location of the A point>;
PUKCL _GF2NEccDbl(nu1ABBase) = <Base of the a and b parameters of the elliptic curve>;
PUKCL _GF2NEccDbl(nu1Workspace) = <Base of the ram location of the workspace>;
...
// vPUKCL_Process() is a macro command, which populates the service name
// and then calls the library...
vPUKCL_Process(GF2NEccDblFast,&PUKCLParam);
if (PUKCL (u2Status) == PUKCL_OK)
{
...
}
else // Manage the error
Constraints
No overlapping between either input and output are allowed. The following conditions must be avoided to ensure the service works correctly:
- nu1ModBase, nu1CnsBase, nu1PointABase, nu1ABBase, nu1Workspace are not aligned on 32-bit boundaries
- {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength+ 12}, {nu1ABBase, 2*u2ModLength + 8}, {nu1Workspace, <WorkspaceLength>} are not in Crypto RAM
- u2ModLength is either: < 12, > 0xffc or not a 32-bit length
- All overlapping between {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1ABase, u2ModLength + 4} and {nu1Workspace, 4*u2ModLength + 28}
Status Returned Values
Returned Status | Importance | Meaning |
---|---|---|
PUKCL_OK | – | The computation passed without problem. |