45.6.2.8 Conversion Timing and Sampling Rate
The following figure shows the ADC timing for one single conversion. A conversion starts after the software or event start are synchronized with the GCLK_ADCx clock. The input channel is sampled in the first half CLK_ADCx period.
The sampling time can be increased by using the Sampling Time Length bit group in the Sampling Time Control register (SAMPCTRL.SAMPLEN). The figure below illustrate the timing conversion with sampling time increased to six CLK_ADC cycles.
Also, the ADC provides offset compensation, see the following figure. The offset compensation is enabled by the Offset Compensation bit in the Sampling Control register (SAMPCTRL.OFFCOMP).
In free running mode, the sampling rate RS is calculated by:
RS = fCLK_ADC / ( nSAMPLING + nOFFCOMP + nDATA)
Where,
- nSAMPLING is the sampling duration in CLK_ADC cycles
- nOFFCOMP is the offset compensation duration in clock cycles
- nDATA is the bit resolution
- fCLK_ADC is the ADC clock frequency from the internal prescaler: fCLK_ADC = fGCLK_ADC / 2^(1 + CTRLA.PRESCALER)
The impact of resolution on the sampling rate is seen in the following two figures, where free-running sampling in 12-bit and 8-bit resolution are compared.
The propagation delay of an ADC measurement is given by: