2.3.2 Using the Library

This topic describes the basic architecture of the Audio 1.0 Function Driver and provides information and examples on its use.

Topics

Name Description
Abstraction ModelDescribes the Abstraction Model of the USB Audio 1.0 Device Library.
Library OverviewThe USB Audio 1.0 Device Library mainly interacts with the system, its clients and function drivers, as shown in the Abstraction Model.The library interface routines are divided into sub-sections, which address one of the blocks or the overall operation of the USB Audio 1.0 Device Library.
How the Library Works This topic describes the basic architecture of the USB Audio 1.0 Device Library and provides information and examples on its use.