2.6.2 Using the Library

This topic describes the basic architecture of the HID Function Driver and provides information and examples on its use.

Topics

Name Description
Abstraction ModelProvides an architectural overview of the USB HID Function Driver.
Library OverviewThe USB HID Device Library mainly interacts with the system, its clients and function drivers, as shown in the Abstraction Model.The library interface routines are divided into sub-sections, which address one of the blocks or the overall operation of the USB HID Device Library.
How the Library WorksThis topic describes the basic architecture of the USB HID Function Driver Library and provides information and examples on its use.