3.2.4.8 USB_HOST_BusSuspend Function

C

USB_HOST_RESULT USB_HOST_BusSuspend(
    USB_HOST_BUS bus
);

Summary

The function suspends the bus. All devices on the bus will be suspended. If bus is specified as USB_HOST_BUS_ALL, all the buses managed by this host will be suspended.

Precondition

The USB_HOST_BusEnable() function should have been called to enable the bus.

Parameters

Parameters Description
bus The bus to be suspended or USB_HOST_BUS_ALL to suspend all buses.

Returns

USB_HOST_RESULT_SUCCESS - if the request was successful.

USB_HOST_RESULT_BUS_NOT_ENABLED - if the bus was not enabled.

USB_HOST_RESULT_FAILURE - An unknown error has occurred.

USB_HOST_RESULT_BUS_UNKNOWN - if the specified bus does not exist in the system

Example

// Suspend the bus 0
USB_HOST_BusSuspend(0);

// Suspend all buses
USB_HOST_BusSuspend(USB_HOST_BUS_ALL);

Remarks

None.