3.7.4.4 USB_HOST_MSD_TRANSFER_CALLBACK Type

C

typedef void (* USB_HOST_MSD_TRANSFER_CALLBACK)(USB_HOST_MSD_LUN_HANDLE lunHandle, USB_HOST_MSD_TRANSFER_HANDLE transferHandle, USB_HOST_MSD_RESULT result, size_t size, uintptr_t context);

Description

USB HOST MSD Transfer Complete Callback

This type defines the type of the callback function that the application must register in the USB_HOST_MSD_Transfer function to receive notification when a transfer has completed. The callback function will be called with the following parameters.

lunHandle - The handle to the LUN from where this notification originated.

transferHandle - the handle to the MSD transfer.

result - result of the transfer.

size - of the transfer.

context - context that specified when this transfer was scheduled.