3.5.2.1 Command Format (Host to BM70/71)
|
Value of Parameter (7...8) |
Parameter Description |
Length – 2 Bytes |
|---|---|---|
0xXXXX | HCI-ISDAP Data Length field Bit 15 1 – Start write continue operation 0 – Normal write operation Bit[14:0] 0x0001:0x7FFF - Packet data length | The Most Significant Bit is repurposed for the continue flag. The maximum value for any HCI-ISDAP write operation can be 32767 bytes in length, but the data sent in each packet is limited based on the packet the BM70/71 can receive (see Read Buffer Size). |
|
Value of Parameter (9) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0x03 | Memory type For the BM70/71, this value is fixed to three, indicating flash memory | — |
|
Value of Parameter (10) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0x00 | Sub-memory type For the BM70/71, this value is fixed to zero, indicating EFLASH memory | — |
|
Value of Parameter (11...14) |
Parameter Description |
Length – 4 Bytes |
|---|---|---|
0xXXXX_XXXX | Starting address of memory within the specified bank where write operations will begin. The most significant 16 bits of the address value represent the bank number. The least significant 16 bits represent the address within the specified bank. | Format is little endian. Example: For an address of 0x0000_1234, the value is sent to the BM70/71 LSB first, 0x34 0x12 0x00 0x00 |
|
Value of Parameter (15...18) |
Parameter Description |
Length – 4 Bytes |
|---|---|---|
0xXXXX_XXXX | HCI-ISDAP data length bit 15 0 – This field represents the number of bytes to write to memory from only this packet. 1 – This field represents the total number of bytes to write to memory in all subsequent write packets. | Format is little endian. Example: For a size of 0x0000_0800, the value is sent to the BM70/71 LSB first, 0x00 0x08 0x00 0x00 |
|
Value of Parameter (19...n) |
Parameter Description |
Length – 1 ... n Bytes |
|---|---|---|
0xXX | Any data to be written to memory. | The length of this field depends on the amount of data the user will write |