2.2.4 Step 4: Disconnect
After completing the flash write process to flash the firmware files, the host needs to disconnect from the flash using the following command to end the programming session.
The opcode to disconnect the connection is 0x0406. The disconnect command terminates an existing connection. For more details on commands, see Commands.
The following flowchart provides a pictorial representation of the steps listed above.