2.2.2 Step 2: Connecting to the Flash
To connect to the Flash via UART in memory programming mode, use the HCI commands. For more details on the HCI command protocol, see General Format of HCI Command Packets (Host to BM70/71). The following commands are primarily used for the Device Firmware update process: