This section provides an overview about the hardware, software and related utility tools required for the demo setup.
The application demo source code relating to this application note is written in an MPLAB X workspace project file and is available for download from the Microchip website. The code is compiled using the Microchip XC8 compiler v2.00 and MPLAB X IDE v3.05.
Use the precompiled RN4678_MCU18_Interface.X.production.hex
file of
the demo or, if required, compile the RN4678_MCU18_Interface project
code
. Ensure the compilation is successful. For additional information
on the source code, related files with description and call graph, refer to the
Appendix B: Source Code. From
MPLAB X, the user can generate call graphs related to specific functions of the demo
code.