The following are the steps to connect the nodes:
- 1.At Node A, press switch S1 to find the peer nodes
in the network. At Node B, press switch S2 to wait for the request from the
connection initiating node/device (Node A).
- 2.The following two figures illustrate
that Node A can start the Inquiry/Discovery process to find the available Bluetooth
devices to enable sending a connection request to the selected device (Node B). Node
B continuously waits for the incoming connection request by not carrying out the
Inquiry process (see Figure 3).
Figure 1. Inquiry/Discovery
Procedure
- 3.Node A now discovers the peer devices
and displays the Inquiring process.
Figure 2. Inquiry/Discovery Procedure in Progress
- 4.Node B waiting for the connection
request from the peer device (Node A). For more details, see the following figure.
Figure 3. Waiting for a Connection Request
- 5.At Node A, the scan result displays a
list of devices found during the Inquiry/Discovery process and the user can select
one of the MAC_ADDR from the list (see the following figure).
Figure 4. Inquiry/Discovery Scan
Result
- 6.After the Inquiry/Discovery process,
the Node B address has to be found from the address list by pressing switch S2.
After finding the Node B address, select the device by pressing switch S1.
- 7.Node A attempts to connect to the
selected device (Node B) if the device Node B MAC address is found in the list.
Otherwise, a new inquiry scan is performed (see the following figure).
Figure 5. Connecting to the
Selected Device/Node
- 8.If the inquiry process fails to find
the expected device, perform the inquiry once again at Node A by pressing switch S2
to find peers again (refer to step 1). For more details, see the following figure.
Figure 6. Display prompting User
to Perform a New Inquiry/Discovery