4.3 Nonvolatile Memory (eFuse)
The ATWILC3000A devices have 768 bits of nonvolatile eFuse memory that can be read by the CPU after device Reset. The eFuse is partitioned into six 128-bit banks (Bank 0 – Bank 5). Each bank has the same bit map (see the following figure). The purpose of the first 108 bits in each bank is fixed and the remaining 20 bits are general purpose software-dependent bits or reserved for future use. Currently, the Bluetooth address is derived from the Wi-Fi MAC address, such that Bluetooth address = Wi-Fi MAC address + 1.
- MAC address.
- Calibration information. For example, crystal frequency offset.
- Other software-specific configuration parameters.
- Invalidate the contents of Bank 1 by programming the Bank Invalid bit field of Bank 1.
- Program Bank 2 with the new MAC address along with the values of ADC Calib (from Bank 1), Frequency Offset (from Bank 1), IQ Amp Correction (from Bank 1) and IQ Pha Correction (from Bank 1). The Used bit field for each corresponding value bit field should also be programmed.
- Validate the contents of Bank 2 by programming the Bank Used bit field of Bank 2.
Each bit field (that is, MAC Addr, ADC Calib, Freq Offset, IQ Amp Correction and IQ Pha
Correction) has its corresponding Used bit field. Each Used bit field is used to
indicate to the firmware that the value in the related bit field is valid. A value of
‘0’ in the Used bit field indicates that the following bit field is
invalid, and a value of ‘1’ programmed to the Used bit field indicates
that the corresponding bit field is valid and can be used by the firmware. By default,
all the ATWILC3000A devices are programmed with the ADC
Calib, IQ Amp and IQ Phase fields of Bank 0. In IC variants where the MAC address is
assigned, the MAC address bit field will be programmed in Bank 0. For more information
on IC marking, refer to Ordering Information and IC Marking.
The matrix table below provides details on how different versions of the firmware handle the IQ Amp Used, IQ Amp Correction, IQ Pha Used and IQ Pha Correction bit fields during Initialization.
| Firmware Version | IQ Amp Used and IQ Pha Used Bit Status | |
|---|---|---|
Device with IQ Amp Used and IQ Pha Used Bit Fields with Value as
‘1’ | Device with IQ Amp Used and IQ Pha Used Bit Fields with Value as
‘0’ | |
| 15.3 or later for WILC Linux 4.5 or later for WILC RTOS | The firmware loads the IQ calibration values from the IQ Amp Correction and IQ Pha Correction bit fields of the corresponding eFuse bank and proceeds with Initialization. | The firmware ignores the values in the IQ Amp Correction and IQ Pha Correction bit fields and proceeds with Initialization. |
| Prior to 15.3 for WILC Linux Prior to 4.5 for WILC RTOS | The firmware does not check for the IQ Amp Used and IQ Pha Used bit fields and proceeds with Initialization. | |