3.1.10 PAL_GetTrxTransmitPowerMax Function
C
int8_t PAL_GetTrxTransmitPowerMax(void)Summary
Gets the transceiver's maximum transmit power in dBm.
Description
This function returns the maximum transmit power that can be set in the Transceiver as per Regulatory region selected in Device support library. User cannot set the Tx power beyond this value
Precondition
None
Parameters
| Param | Description |
|---|---|
| Output | Integer value holding the maximum transmit power of the transceiver that can be set by higher layer |
Returns
None
Example
int8_t txpwrMax = INT8_MAX;
txpwrMax = PAL_GetTrxTransmitPowerMax();
printf ("Maximum Tx Pwr Value - %i", txpwrMax);Remarks
Transmit Power Max value as per Regulatory region