3.1.3 PAL_TimerGetId Function
C
PAL_Status_t PAL_TimerGetId(TimerId_t *timer_id)Summary
Gets the Timer Id
Description
Returns a timer id to be used before starting a timer
Precondition
PAL_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| timer_id | Value of the id returned by the function |
Returns
PAL_SUCCESS - If there is a unused timer
PAL_FAILURE - If there are no timer unused
Example
TimerId_t appTimer;
//Get the Id for the sotware timer instance
PAL_TimerGetId(&appTimer);Remarks
None