3.8.2 Temperature Measurement
When triggering a temperature measurement, the AD converter of the ATA8210/15 operates as a temperature sensor in the range of -40°C to +125°C with a resolution of 1K. The temperature is measured on a specific temperature measurement channel with fLO = 422 MHz. The result of the AD converter is provided in the TEMPH and TEMPL hardware registers, then copied to the calib.sramTEMPH/L SRAM variables by the firmware.
In a subsequent step, a temperature value is calculated and stored to the calib.tempMeas SRAM variable. The valid range of tempMeas is 0-175. Calculate the actual temperature in °C by using the following formula:
T = tempMeas – 50 (2)
Equation parameters:
T – Current temperature [°C]
tempMeas – Content of the calib.tempMeas SRAM variable
Address | Name | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|---|---|
0x02D9 | sramTEMPH | Temperature high byte | |||||||
0x02DA | sramTEMPL | Temperature low byte | |||||||
0x02DB | tempMeas | 8-bit temperature measurement result (valid range 0-175) | |||||||
Use the result of the calculation as input for the XTO temperature compensation (RF calibration). See RF Calibration from Related Links.
Use the Read SRAM/Register SPI command to read out the calculated temperature from the calib.tempMeas SRAM variable.
A temperature measurement process can be triggered at the following time points:
- After power-on during system initialization when enabled in eepConfValid.confInitFlags.TempMeas.
Address | Name | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|---|---|
0x0008 | confInitFlags | — | TempMeas | SRC | FRC | — | — | — | — |
- During the periodic self-check in PollingMode or during a self-check that is started by using the
Calibrate and CheckSPI command if enabled in eepTrxCal.calConf1.EN_TEMP_MEAS.
| Address | Name | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|---|---|
| 0x001C | calConf1 | — | EN_TEMP_MEAS | EN_SRCCAL | EN_FRCCAL | — | — | — | EN_REGREFRESH |
- From IDLEMode via the
Calibrate and CheckSPI command if bit EN_TEMP_MEAS in tuneCheckConfig is set to ‘1’. See Calibrate and Check from Related Links.
| Name | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|---|
| tuneCheckConfig | — | EN_TEMP_MEAS | EN_SRCCAL | EN_FRCCAL | EN_VCOCAL | — | EN_SELFCHECK | — |
Setting the TEMP_MEAS bit within the eepEventConf.cmdRdyConf command ready variable to ‘1’ raises a command ready (CMD_RDY) event on the PB6 EVENT pin when finishing the temperature measurement process.
| Address | Name | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|---|---|
| 0x0096 | cmdRdyConf | — | TEMP_MEAS | SRC_CAL | FRC_CAL | VCO_CAL | RF_CAL | SELFCHECK | — |
The temperature measurement requires additional time. See Timing Characteristics from Related Links.