4.5.1.1 Data FIFO Overview
The Data FIFO (DFIFO) is a 32-byte deep register bank that stores data with first-in-first-out functionality. The DFIFO has two read and two write interfaces:
- AVR bus read and write access
- Direct write access from the RX buffer
- Direct read access not connected in ATA8210/15
The DFIFO additionally implements a configurable fill level status bit with maskable interrupt signaling. Read attempts to an empty DFIFO (underflow) and write attempts a full DFIFO (overflow) are indicated by error flags (DFS.DFUFL and DFS.DFOFL) in the user interface. An error IRQ is triggered if masked in DFI.DFERIM.
A special feature of the DFIFO is the telegram length registers (DFTLH/DFTLL). These registers can be used in DFC.DFDRA = 0 mode to read the number of received bits of the last telegram. This is helpful for unknown telegram lengths, especially if a telegram is not byte-aligned (number of bits is not divisible by 8). The telegram length is written to the registers by the RX buffer once after an EOT is received. The registers are not continuously updated during reception.
The access mode of the DFIFO is configured by the DFC.DFDRA register bit. If the bit is set to ‘0’, the RX buffer can write to the DFIFO via the direct write interface while the AVR can only read from the DFIFO. This mode must be selected if the ATA8210/15 is receiving data. If the DFC.DFDRA bit is set to ‘1’, the AVR can only write to the DFIFO.
The DFIFO can trigger an interrupt if a certain fill level is reached. The interrupt can be switched on by setting the DFIFO fill level interrupt mask bit (DFI.DFFLIM) to ‘1’. The required fill level can be configured in the DFIFO fill level configuration register (DFC.DFFLC) to any value between 0 and 32. Once the configured fill level is reached (in DFDRA = 0 mode after a byte was written to the DFIFO, in DFDRA = 1 mode after a byte was read from the DFIFO), the DFIFO fill level reached status bit (DFS.DFFLRF) is set and the interrupt is triggered if enabled.
The current fill level can be read at any time in the DFIFO fill level register (DFL.DFFLS).
The AVR can access the data in the DFIFO by writing or reading the DFIFO data register (DFD). The user has to set the DFC.DFDRA correctly to allow either write or read access by the AVR.
The current read and write pointer addresses can be read from the DFRP and DFWP registers, respectively. The AVR also has write access to these registers, but manual pointer manipulations must be handled with care and are mainly implemented for the purpose of debugging.
The DFIFO is reset when activated in the corresponding power reduction register PRR2.PRDF or by
writing a ‘1’ to the DFL.DFCLR bit. See Sleep Modes and Active Power
Reduction from Related Links.
For more details on the description of the required register bits, see Data FIFO Register Description from Related Links.